EEO#.STATUS
Description
Reports the state of the Output - Encoder Emulation. The possible values are:
Value | Name | Description |
---|---|---|
0 | Disabled | EEO#.SOURCE is 0 (None). |
1 | Operational | EEO signal is output on the EEO’s connector. |
10 | Configuration Conflict | EEO#.SOURCE is not 0 (None) but the connector configuration (X#.MODE) is not set to EEO. |
11 | Faulted | EEO is configured correctly but not working (e.g. due to losing connection to an SFA that is used to output the EEO signal). |
If EEO#.STATUS is 11 (Faulted), DRV.CLRFAULTS will reinitialize the EEO in an attempt to get it operational again, even if EEO#.FAULTAXIS is set up to not create a fault on an axis.
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-09-02-000 |
General Information
Type | Read Only |
Units | N/A |
Range | 0 to 11 |
Default Value | N/A |
Data Type | Integer |
See Also | |
Stored in Non-Volatile Memory | No |
Variants Supported
All variants are supported.
Fieldbus Information
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
---|---|---|---|---|---|---|---|
EEO1.STATUS |
4600h |
0ah |
Unsigned8 |
- |
- |
Read only |
No |
EEO2.STATUS |
4601h |
0ah |
Unsigned8 |
- |
- |
Read only |
No |
EEO3.STATUS |
4603h |
0ah |
Unsigned8 |
- |
- |
Read only |
No |
EEO4.STATUS |
4606h |
0ah |
Unsigned8 |
- |
- |
Read only |
No |
ID |
Instance |
Attribute |
Name |
Data Type |
Access |
User Mappable |
---|---|---|---|---|---|---|
32055 |
1 |
32055 (0x7d37) |
EEO1.STATUS |
Unsigned8 |
Read Only |
Yes |
32056 |
1 |
32056 (0x7d38) |
EEO2.STATUS |
Unsigned8 |
Read Only |
Yes |
32057 |
1 |
32057 (0x7d39) |
EEO3.STATUS |
Unsigned8 |
Read Only |
Yes |
32058 |
1 |
32058 (0x7d3a) |
EEO4.STATUS |
Unsigned8 |
Read Only |
Yes |
Parameter |
PNU |
Data Type |
Access |
Units |
---|---|---|---|---|
EEO1.STATUS |
32055 |
Unsigned8 |
Read Only |
- |
EEO2.STATUS |
32056 |
Unsigned8 |
Read Only |
- |
EEO3.STATUS |
32057 |
Unsigned8 |
Read Only |
- |
EEO4.STATUS |
32058 |
Unsigned8 |
Read Only |
- |